Embedded Security Made Easy: Protection from Product Piracy and IP Theft for Capital Equipment

Jul 20, 2015 | Technology Media

Munich, Germany – July 20, 2015 – Industrial automation, medical equipment, electronic components – plagiarism of capital equipment requires effective prevention, such as embedded security solutions from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY). According to the OECD, counterfeiting and piracy costs add up to around 638 billion US dollars annually. The new OPTIGA™ Trust E offers an easily implementable solution to protect manufacturers’ valuable IP from being attacked, analyzed, copied and modified. Enhanced authentication as well as secured storage of software codes and product data improve network and supply chain management – particularly in the context of Industry 4.0. And help manufacturers of high value goods to safeguard their IP and protect their brand through assured quality and safety of their products.

Research for built-in copy protection is also conducted by the Fraunhofer Institute for Applied and Integrated Security (AISEC) in Garching, Germany. “Most companies have no idea just how easy it is to copy their products,” says Bartol Filipovic, head of the Product Protection and Industrial Security department at the Fraunhofer Institute. “Encrypted software is not enough to protect standard products or machine codes. The software codes must be ideally stored in protected hardware.”

Thanks to the smart security features provided by the OPTIGA Trust E, it is also possible to track the source of spare parts. This benefits manufacturers of wind mills, for example, who want to control after-sales markets of the installed systems or components in order to avoid damage and warranty claims caused by unqualified service or fake parts. The security technology is already integrated into the intelligent power module MIPAQ™ Pro from Infineon. First implementation has been realized at an international wind mill manufacturer.

The OPTIGA Trust E comes with an advanced pre-programmed security controller built on Elliptic Curve Cryptography greatly enhancing overall system security. Furthermore, the easy-to-integrate, cost effective “out of the box” solution features key and certificate management and includes operating software. Moreover, it comes with complete system integration support. The extended temperature range of -40 to +85 °C combined with a standardized I²C interface and small USON-10 footprint allows integration into a variety of embedded projects. Beyond that, it supports authentication of products that rely on the new USB Type-C standard.

The OPTIGA Trust E is already available in volume quantities.

IP protection is also a major issue for increasingly connected industrial systems. Infineon has developed a broad range of easy-to-deploy semiconductor technologies to counter growing security threats. The OPTIGA product family for embedded security includes components from authentication solutions (OPTIGA Trust) to advanced implementations (OPTIGA TPM) protecting integrity, authenticity and confidentiality of information to enable security in the Internet of Things (IoT). Further information is available at: www.infineon.com/iot-security

About Infineon

Infineon Technologies AG is a world leader in semiconductors. Infineon offers products and system solutions addressing three central challenges to modern society: energy efficiency, mobility and security. In the 2014 fiscal year (ending September 30), the company reported sales of Euro 4.3 billion with about 29,800 employees worldwide. In January 2015, Infineon acquired US-based International Rectifier Corporation, a leading provider of power management technology, with revenues of USD 1.1 billion (fiscal year 2014 ending June 29) and approximately 4,200 employees.

Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Follow us: twitter.com/Infineonfacebook.com/Infineonplus.google.com/+Infineon

Information Number

INFCCS201507-072

Press Photos

  • The new OPTIGA™ Trust E offers an easily implementable solution to protect manufacturers' valuable IP from being attacked, analyzed, copied and modified. This helps manufacturers of wind mills, for example, to avoid damage and warranty claims caused by unqualified service or fake parts.
    The new OPTIGA™ Trust E offers an easily implementable solution to protect manufacturers' valuable IP from being attacked, analyzed, copied and modified. This helps manufacturers of wind mills, for example, to avoid damage and warranty claims caused by unqualified service or fake parts.
    OPTIGA-Trust-E

    JPG | 1.32 mb | 2126 x 1606 px