New LTE Low Noise Amplifiers and LNA banks from Infineon improve data rates of smartphones by up to 96 percent, thus improving user experience

Jan 27, 2014 | Market News

Neubiberg, Germany – January 27, 2014 – Infineon Technologies today introduced a new series of LTE Low Noise Amplifiers (LNA) and Quad LNA banks specially designed to enhance the data rate in smartphones.

LTE (also 4G) is the latest standard for wireless communication and allows for data rates up to 300 Mbit/s – compared to 56 Mbit/s in the latest UMTS (3G) release. This results in mobile internet connection without notable loading times and dramatically increases smartphone users’ comfort and satisfaction.

However, meeting user expectations for high data rates in LTE is challenging in today’s mobile devices. The increasing complexity of the RF front end results in the usage of more RF components (e.g. switches, diplexers and dividers). This leads to increasing losses over the whole system and deterioration of the signal-to-noise ratio (SNR). Furthermore, the distance between antennas and the RF transceiver leads to additional line losses that also negatively affect SNR and consequently also data rate.

Infineon’s BGA7x1N6 and BGM7xxxx4L12 families provide low noise figure, the exact gain and high linearity needed to help smartphone designers overcome these challenges. The products are based on the company’s advanced SiGe (Silicon Germanium) chip technology and include built-in ESD protection.

The new LNAs and LNA banks are located in both the diversity and main antenna path of the phone, in order to increase system sensitivity and assure the best possible user experience. They allow for data rates that are up to 96 percent higher than in solutions without LNAs to fully exploit the potential of LTE. High linearity of the new device series assures optimal signal reception even in conditions of poorly isolated antenna and long line losses between antenna and transceiver. The typical sensitivity improvement of 3.4 dB compared to systems without LNAs is achieved in devices with a package size 70 percent smaller (1.1 mm x 0.7 mm) than previously available LNAs and 61 percent smaller (1.9 mm x 1.1mm) than previously available LNA banks.

Availability and Packaging

Infineon offers three LTE LNAs and seven Quad LNA bank families to address the required band configurations for different world regions. Each letter in the series denotes a different frequency band (L for the low, 0.7 to 1.0 GHz band; M for mid, 1.7 to 2.2 GHz band; and H for high, 2.3 to 2.7 GHz band).

  • BGA7L1N6
  • BGA7M1N6
  • BGA7H1N6
  • BGM7LLHM4L12
  • BGM7LLMM4L12
  • BGM7MLLH4L12
  • BGM7MLLM4L12
  • BGM7LMHM4L12
  • BGM7HHMH4L12
  • BGM7MHLL4L12

The devices are shipped in ROHS compliant TSNP-6-2 or TSLP 12-4 plastic packages.

Additional technical information on the BGA7x1N6 LTE LNAs and BGM7xxxx4L12 Quad LNA banks family is available at www.infineon.com/rfmmic

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2013 fiscal year (ending September 30), the Company reported sales of €3.84 billion with around 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).Further information is available at www.infineon.com

Information Number

INFPMM201401.017