New member of the EiceDRIVER™ family: 1EDI Compact Driver with Coreless Transformer Technology for applications up to 1200 V

Nov 26, 2013 | Technology Media

Neubiberg, Germany – November 26, 2013 – At this year's SPS IPC Drives trade fair for electrical automation, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) will present its new 1EDI EiceDRIVER™ Compact Single Channel Gate Driver for applications with isolation voltages of up to 1200 volts. The galvanically isolated driver components are based on the Coreless Transformer Technology developed by Infineon, which enables output currents of up to 6 amperes on separate output pins. The basic system includes UVLO (under voltage lockout) for IGBTs and MOFETs as well as an active shutdown in the event that the driver is not connected to the power supply. The 1EDI drivers are supplied in a compact DSO-8 housing and can be used at ambient temperatures of up to 125°C in applications such as industrial drives, inverters, welding equipment, induction cooking appliances and power supplies for servers or telecommunications.

“With the 1EDI driver IC, we are further expanding our extensive range of driver ICs – which are differentiated according to applications as well as functionality – into the compact area. As with the 2EDL Compact, the new driver component is also aiming at the mass market both in the consumer as well as the industrial area,” says Oliver Hellmund from Infineon, who is responsible for marketing the EiceDRIVERTM. “The 1EDI Compact stands for exceptionally robust and simultaneously very secure control of high-voltage power semiconductors. Our compact driver range now covers all applications for power semiconductors with functional isolation.” The 1EDI driver ICs are offered in eight variants that can be operated at up to voltages of 1200 volts and are designed for use in applications with either IGBTs or MOSFETs.

The new EiceDRIVER™ components are the first driver ICs to achieve a value of 100kV/µs for the CMTI (common mode transient immunity). Both the MOSFET as well as one IGBT driver supply six amperes of output current. The MOSFET driver is optimized for use with power semiconductors that are based on CoolMOS™ technology. Due to lower induction loss, the EiceDRIVER™ thus enables an additional gain in efficiency of 0.5 percent with the latest generation CoolMOS C7. Further IGBT only variants with 4, 2 and 0.5 amperes are in preparation. These five variants have a separate output for charging and discharging the gate. An additional three variants are structured to limit the gate voltage (active Miller clamp) and provide 3, 2 and 1 amperes of output current.

In addition to the compact class, the EiceDRIVER™ family also includes the EiceDRIVER™ Enhanced class which offers increased functionality both for the industrial as well as partially the consumer sectors.

Availability and additional information

Samples of the 1EDI EiceDRIVER™ for MOSFETs and IGBTs with 6 amperes of output current are available now; the corresponding Customer Evaluation Board can be ordered as of January 2014. Production start for both these variants will presumably begin in March 2014. The other drivers are intended to be available as samples in the first quarter of 2014; production is planned to begin in the second quarter of 2014. More detailed information about the entire driver IC family is available under www.infineon.com/eicedriver. Infineon is presenting the new 1EDL EiceDRIVER™ from November 26 to 28, 2013 at the SPS IPC Drives trade fair in Nuremberg in Hall 1, Stand 328. Further information on fair highlights is available in the Internet.

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2013 fiscal year (ending September 30), the Company reported sales of €3.84 billion with around 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).Further information is available at www.infineon.com

Information Number

INFIPC201311.011

Press Photos