A tip for television buyers - Infineon chips substantially reduce power consumption in flat-screen TVs

Sep 4, 2007 | Business & Financial Press

Neubiberg, September 4, 2007 - Infineon Technologies (FSE/NYSE: IFX), the world market leader in power electronics, today warned of the growing demand for power in the consumer electronics sector and highlighted products capable of increasing energy efficiency. Compared to conventional CRT televisions, which need just 50-70 watts to deliver brilliant images, some of today’s LCD flat-screen TVs consume more than 300 watts of power. The main reason for this high power consumption is the backlighting that this panel technology needs to deliver a contrast-rich image. However some models of television, including the Individual 46 and Individual 40 Selection DR+ sets from German TV maker Loewe, show that greater power economy is possible. These two LCD flat screens consume 165 and 150 watts respectively and currently head the LCD television energy efficiency rankings for models with screen sizes above 101 cm (www.topprodukte.at). These TVs contain a number of Infineon power supply chips that help to ensure that as little energy as possible is converted into heat.

“Electronic components in typical consumer electronics power supplies waste around 10 to 15 percent of the energy. By contrast, our chips perform around 25 percent more efficiently,” says Andreas Urschitz, who heads Infineon’s power management chips business. “The cost of this waste can really mount up, running to as much as Euros 40 a year for a TV set alone.”

According to market researchers iSuppli, the demand for large, flat-screen televisions will continue to grow. World sales of displays of this type will likely exceed 350 million this year and are expected to rise to almost 600 million in 2011, accounting for 65 percent of all TV sets sold.

Infineon’s power supply chips are used to convert mains AC voltage into DC voltage and to produce a number of different DC voltages as constantly as possible.

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, communications and security. In fiscal year 2006 (ending September), the company achieved sales of Euro 7.9 billion (including Qimonda sales of Euro 3.8 billion) with approximately 42,000 employees worldwide (including approximately 12,000 Qimonda employees). With a global presence, Infineon operates through its subsidiaries in the US from Milpitas, CA, in the Asia-Pacific region from Singapore, and in Japan from Tokyo. Infineon is listed on the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.

Information Number

INFXX200708.085

Press Photos

  • The LCD flat screens Individual 46 and Individual 40 Selection DR+ from German TV maker Loewe currently head the LCD television energy efficiency rankings (www.topprodukte.at) for models with screen sizes above 101 cm thanks to a number of Infineon power supply chips.
    The LCD flat screens Individual 46 and Individual 40 Selection DR+ from German TV maker Loewe currently head the LCD television energy efficiency rankings (www.topprodukte.at) for models with screen sizes above 101 cm thanks to a number of Infineon power supply chips.
    INFXX200708-085

    JPG | 436 kb | 2268 x 2700 px