Infineon launches single chip TV Tuner IC with integrated RF and IF functions that offers lower power consumption, half the footprint area with a superior cost position

Jun 22, 2006 | Technology Media

Munich, Germany – June 22, 2006 – Infineon Technologies AG (FSE/NYSE: IFX), a leading supplier of TV tuner ICs, introduced today an economic, low power tuner IC, Taifun TUA6039. The TUA6039 integrates the complete RF (Radio Frequency) and IF (Intermediate Frequency) functions on a single chip, leading the evolution of smaller and more cost effective digital TV tuner ICs without compromise to performance.
 
The TUA6039 has only half the footprint area of the conventional RF + IF tuner solution. The highly integrated IC provides a reliable solution for tuner, set-top box and TV manufacturers, offering a 50 percent reduction in board space and power consumption compared to previous generation. This makes the TUA6039 an ideal upgrade path for customers that are currently using Infineon`s two-chip solution, consisting of TUA6034 (RF multimedia tuner) and TDA6192 (IF amplifier).
 
The TUA6039 is manufactured using a bi-polar process and is well-suited for stationary broadcast receivers where both low cost and lower power consumption are major design requirements in this highly competitive market. TUA6039 is a full 3-band RF tuner IC with integrated IF AGC (Automatic Gain Control) amplifier and PLL. This low power tuner IC operates between 3V and 5V supply voltage with a power consumption of only 330mW (typical) compared to about 600mW for similar competing solutions. The high level of system integration enables more cost effective tuner solutions and reduces development cycle times that allows for faster time to market.  All major analog and digital standards for terrestrial and cable applications like PAL, SECAM, NTSC, DVB-C, DVB-T, T-DMB, DAB, ISDB-T and ATSC are supported by TUA6039.
 
The flexibility to operate at supply voltages ranging from 5V to 3V allows manufacturers of tuner modules the freedom to adjust the tuner modules to the various receiver system power requirements. System power consumption is further reduced with the build-in stand-by mode function and bus controlled power-down mode.
 
Infineon has successfully introduced several generations of tuner ICs over the last few decades which have been designed into more than 60 percent of the worldwide digital terrestrial receivers.  In addition, the company’s analog and digital tuner IC’s are used in one of every four TV tuners in the world.  Infineon is leveraging on its RF core competency that ultimately plays a key role in enabling the digital age of terrestrial television.
 
“The latest market driven trends in developing digital television receivers are the competencies to reduce the footprint of the tuner module while delivering higher performance and lower power consumption at significantly reduced costs,” said Giuseppe Calarco , General Manager of the Tuner Systems business unit at Infineon's communication Solutions business group. “The launch of the TUA6039 shows that Infineon is continuing to expand its expertise in analog and RF chip design and manufacturing to support its customers with strategic products for the TV tuner market.”
 
Availability
 
Samples of TUA6039 in Green PG-VQFN-48 packages are already available, with volume production planned for 3 rd quarter 2006. Infineon will also make available a complete TV Tuner reference design with TUA6039 that will provide added value to customers by reducing their development costs and time to market. For portable applications requiring extreme low power consumption, Infineon also offers the recently announced TUA 6041/ TUA6045 Tuner ICs using BiCMOS process.

About Infineon

Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for automotive, industrial and multimarket sectors, for applications in communication, as well as memory products through its subsidiary Qimonda. With a global presence, Infineon operates through its subsidiaries in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2005 (ending September), the company achieved sales of Euro 6.76 billion with about 36,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com. Further information on Qimonda is available at www.qimonda.com .

Information Number

INFCOM200606.070

Press Photos

  • Infineon launches single chip TV Tuner IC with integrated RF and IF functions that offers lower power consumption, half the footprint area with a superior cost position<br><br>Infineon integriert RF- und IF-Funktionen in Single-Chip TV-Tuner-IC: Geringe Leistungsaufnahme, halb so große Platinenfläche, überragendes Kosten/ Nutzen-Verhältnis
    Infineon launches single chip TV Tuner IC with integrated RF and IF functions that offers lower power consumption, half the footprint area with a superior cost position

    Infineon integriert RF- und IF-Funktionen in Single-Chip TV-Tuner-IC: Geringe Leistungsaufnahme, halb so große Platinenfläche, überragendes Kosten/ Nutzen-Verhältnis
    TUA 6039 TP

    JPG | 820 kb | 1535 x 1063 px

  • Infineon launches single chip TV Tuner IC with integrated RF and IF functions that offers lower power consumption, half the footprint area with a superior cost position<br><br>Infineon integriert RF- und IF-Funktionen in Single-Chip TV-Tuner-IC: Geringe Leistungsaufnahme, halb so große Platinenfläche, überragendes Kosten/ Nutzen-Verhältnis
    Infineon launches single chip TV Tuner IC with integrated RF and IF functions that offers lower power consumption, half the footprint area with a superior cost position

    Infineon integriert RF- und IF-Funktionen in Single-Chip TV-Tuner-IC: Geringe Leistungsaufnahme, halb so große Platinenfläche, überragendes Kosten/ Nutzen-Verhältnis
    TUA 6039 FP

    JPG | 926 kb | 1535 x 1063 px