Infineon Makes UMTS Phones Usable Worldwide

Jun 14, 2005 | Technology Media

Munich, Germany – June 14, 2005 – New features such as fast data transmission and new applications like recording, sending and receiving video clips or receiving television while on the move are generally associated with the new UMTS (Universal Mobile Telecommunications System) mobile radio standard. But “universal” does not automatically mean that a UMTS handset will also work anywhere in the world. A total of six frequency blocks have been defined for providing UMTS services worldwide. To make next-generation mobile phones “universal” in the truest sense of the word, Infineon Technologies AG (FSE/NYSE: IFX) recently introduced a new chip which accommodates the transmit and receive electronics for all six frequency bands in a footprint measuring only 5mm on 5mm. SMARTi 3G is the name of the smart chip, which Infineon unveiled this week at an industry conference in California.

Mobile radio devices include a radio-frequency transceiver which is responsible for transmitting and receiving the signals. The term “transceiver” is a composite formed from the two words “transmitter” and “receiver”. Prior to transmission, the SMARTi 3G converts the electronic signals for voice or data into high-frequency signals and amplifies them. It converts received high-frequency signals into low-frequency electronic signals, which are then converted into voice and data in the phone’s processor.

Samples of the SMARTi 3G are already available and leading manufacturers worldwide are integrating the chip into the next generation of UMTS handsets. Infineon is a major player when it comes to transmit and receive electronics for mobile phones. Last year the company sold more than 170 million transceiver chips. This means that roughly one in four mobile phones worldwide operates with an Infineon transceiver.

The SMARTi 3G chip is manufactured using silicon process technology with microstructures of only 130 nanometers (a human hair is 500 times thicker). At 7.2 megabits per second, it meets the requirements of next-generation UMTS telephones for data transmission from the base station to the mobile device. The chip was developed in Germany and Austria and is produced in France.

About Infineon

Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for automotive, industrial and multimarket sectors, for applications in communication, as well as memory products. With a global presence, Infineon operates through its subsidiaries in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2004 (ending September), the company achieved sales of Euro 7.19 billion with about 35,600 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at

Information Number


Press Photos

  • UMTS phones incorporating SMARTi 3G can be used in Europe, Asia, North America and Japan. Mobile phone's design study: Design Afairs.
    UMTS phones incorporating SMARTi 3G can be used in Europe, Asia, North America and Japan. Mobile phone's design study: Design Afairs.
    Press Photo

    JPG | 1.22 mb | 2126 x 1519 px

    Press Photo

    JPG | 14 kb | 160 x 114 px