ADSL2+ Chip from Infineon Sets New Standards for Power Consumption and System Costs

Mar 31, 2005 | Technology Media

Munich, Germany – March 31, 2005 – The German semiconductor manufacturer Infineon Technologies AG has introduced the world’s smallest and most economical chip for “ADSL2+” - the DSL data network of the future. This chip enables telecommunications companies to boost the number of super-high-speed DSL connections that they offer to their customers by approximately one third - without additional investments for cooling or for power supply and without changing cabinet sizes. With ADSL2+, which is expected to be launched as a service on a wide scale in 2006, a conventional telephone connection is sufficient to surf the Internet, receive multiple television channels and place a telephone call all at the same time.

“With the new semiconductor chip for future DSL central offices, Infineon Technologies is underscoring its leading role in the booming market for the chips that are being used in broadband data networks,” emphasizes Christian Wolff, Vice President Communications Business Group and General Manager Wireline Access Business Unit at Infineon. At the beginning of 2005, there were approximately 100 million DSL connections throughout the world. Approximately 40 percent of these connections were added last year. This growth is expected to continue over the next few years. In the process, the new ADSL2+ standard is to replace the current DSL connections soon. With ADSL2+, data can be transmitted at up to 25 megabits per second. This is approximately ten to twenty times faster than the DSL connections that are typically in use today, and it is sufficient to transmit several high-definition television broadcasts, Internet data and inexpensive Internet telephone calls simultaneously.

Less Heat – More Connections Within the Same Space



The new “GEMINAX PRO” ADSL2+ chipset from Infineon offers DSL central offices performance features that are unmatched to date. Power consumption is about 30 percent lower than is the case with conventional chips, and a correspondingly lower amount of heat is produced. Thanks to these features and to the small overall size, it is possible to install the chips in switching systems at much higher densities without requiring any additional cooling. Over all, GEMINAX PRO now makes it possible to install approximately one third more ADSL2+ connections without increasing the amount of cabinet space that is required.

The “switched-mode” technology that is used in GEMINAX PRO is already being employed widely in portable audio devices (such as MP3 players) due to its extremely low power consumption levels. Through a multitude of technological innovations, Infineon’s developers have now succeeded in adapting and advancing this technology for broadband applications, although the requirements in this area are much more stringent and the frequency that is used is 100 times higher. The first prototypes for the new chip will be shipped in May, and volume production will begin in autumn 2005.

About Infineon



Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for automotive, industrial and multimarket sectors, for applications in communication, as well as memory products. With a global presence, Infineon operates through its subsidiaries in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2004 (ending September), the company achieved sales of Euro 7.19 billion with about 35,600 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.

Information Number

INFCOM200503.048

Press Photos

  • GEMINAX PRO is the industry`s highest-integration and lowest-power ADSL2+ chipset.
    GEMINAX PRO is the industry`s highest-integration and lowest-power ADSL2+ chipset.
    Press Photo

    JPG | 132 kb | 1535 x 1063 px

    Press Photo

    JPG | 5 kb | 160 x 111 px

  • Consisting of a 16-channel ADSL2+ Digital Front End (DFE) and a 4-channel Analog Front End (AFE), with integrated low-power Class D line drivers, the GEMINAX PRO chipset reduces power dissipation, footprint and overall system costs by up to 30 percent, in comparison to other chipsets currently available.
    Consisting of a 16-channel ADSL2+ Digital Front End (DFE) and a 4-channel Analog Front End (AFE), with integrated low-power Class D line drivers, the GEMINAX PRO chipset reduces power dissipation, footprint and overall system costs by up to 30 percent, in comparison to other chipsets currently available.
    Press Photo

    JPG | 292 kb | 1535 x 1063 px

    Press Photo

    JPG | 9 kb | 160 x 111 px

  • GEMINAX PRO is the industry`s highest-integration and lowest-power ADSL2+ chipset.
    GEMINAX PRO is the industry`s highest-integration and lowest-power ADSL2+ chipset.
    Press Photo

    JPG | 425 kb | 1535 x 1063 px

    Press Photo

    JPG | 11 kb | 160 x 111 px