Infineon Brings Safety into Car Tires

Jun 23, 2003 | Market News

Munich – June 23, 2003 – Infineon Technologies (FSE/NYSE: IFX) increases the safety on the road. The company’s solution portfolio now also includes tire pressure sensors, which collect data such as pressure, temperature, and motion and transmit them to a dashboard display over a radio link. Based on information published by the German Federal Statistical Office, insufficient pressure in car tires caused about 25 per cent of all traffic accidents in 2002 that occurred due to technical defects. With the yet closed acquisition of Norwegian manufacturer SensoNor Infineon is significantly strengthening its sensor business and broadens its range of competencies within the field of automotive electronics with another key safety component. In the segment of tire pressure sensors, Infineon now is the worldwide market leader and has concluded long-term agreements with leading car manufacturers.

Fuel consumption reduced by up to five per cent



By using a tire pressure monitor system, drivers can improve their safety and riding comfort. This eliminates the need to check the air pressure at a gas station, since critical changes will automatically issue a warning message on the display. Proper tire pressure will optimize the rolling resistance, lower the fuel consumption, and reduce tire wear. According to German TÜV-Nord institute, half a bar of missing pressure will increase the fuel consumption by five per cent. However, insufficient tire pressure also affects the car’s roadability. Steering becomes more difficult, and the stopping distance becomes longer. Due to the increased rolling resistance with poor tire pressure, the tires will also be exposed to more flexing and heat up faster until they are no longer able to withstand the stress and burst. Truck tires can even catch fire.

It is planned to use the information delivered by the sensors not only to display a warning, but also to feed them into the controllers of other safety systems such as ESP or ABS. In the USA, tire pressure monitoring system will be required by law from November of this year: By end of 2006, every new U.S. car must be equipped with such a system.

In addition to the sensors, the monitoring system comprises a microcontroller for each tire, which processes the data, and a transmitter, which sends the information to the controller in the engine compartment over an RF (Radio Frequency) link. Infineon plans to integrate these discrete components into a single unit and launch it in two to three years’ time. Even systems that operate without a battery should be feasible at the end of decade. Currently, tire pressure monitor systems are commercially available as retrofit versions for 200 to 400 Euro. An increasing number of manufacturers offer their cars factory-equipped with such systems, even in the medium-range segment.

About Infineon



Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2002 (ending September), the company achieved sales of Euro 5.21 billion with about 30,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at http://www.infineon.com.

Information Number

INFXX200306.093

Press Photos

  • Infineon Brings Safety into Car Tires
    Infineon Brings Safety into Car Tires
    TPM module

    JPG | 99 kb | 1535 x 1063 px

    TPM module

    JPG | 10 kb | 160 x 111 px