Technology Innovation: Neurological Biosensor Chip from Infineon Technologies Can Measure Electrical Activity in Living Cells, Breakthrough Promises New Techniques for Neuroscience and Drug Development

Feb 11, 2003 | Market News

Munich, Germany and San Francisco, Calif. – February 11, 2003 – Researchers at Infineon Technologies have succeeded in cooperation with the Max Planck Institute in directly connecting a newly developed biosensor chip with living nerve cells and reading electrical signals produced by the cells. This breakthrough technology, which Infineon calls a “Neuro-Chip“, will allow scientific researchers to gain new insights into the biologic function of neurons, nerve tissue, and organic neural networks. In the field of drug development, the Neuro-Chip ultimately will enable tests of the effects of new pharmaceutical compounds on living neurons, contributing to greater efficiency and productivity in research.

Infineon described the Neuro-Chip development in a paper presented today at the International Solid State Circuits Conference (ISSCC) 2003, a highly respected global forum for new developments in semiconductors. The research findings include the first report on measurements of electrical signals from live neurons. Working with the renowned Max Planck Institute of Biochemistry, Infineon’s project partner and one of the world’s leading institutes for bioscience research, the researchers have recorded electrical signals from the neurons from snail brains.

Neurons are the specialized cells that make up the nervous systems of all living things. Nerve tissues, comprised of many associated nerve cells, are the principal component of the brain and spinal cord. Nerve cells communicate with each other through electrical pulses, so the ability to read these signals and record them in a computer system holds the promise of new insights into neurological processes.

“Concerning the signal-to-noise ratio this chip operates close to elementary physical limits,” said Dr. Roland Thewes, the Senior Director responsible for biosensor chip activities within the Corporate Research Center at Infineon Technologies. “Infineon is able to draw on 50 years of knowledge in chip making to develop biochips that bring the advantages of silicon technology to biochemistry and new drug research. With the Neuro-Chip, we are laying the groundwork for advances in scientific understanding.”

Infineon has collaborated since mid-2000 with researchers at the Max Planck Institute (MPI) for Biochemistry in Martinsried, near Munich, on development of the Neuro-Chip and associated test system. Infineon is principally responsible for the semiconductor technology development, and the MPI provides its specialized know-how in the field of neuron-chip-interfacing.

Professor Dr. Peter Fromherz, Director of the Max Planck Institute for Biochemistry in Martinsried, Germany, comments: “That our long-lasting basic research on neuron-semiconductor interfaces now sees a high-tech chip, is like a dream coming true. Infineon's development of cutting edge microelectronics may be a pre-condition for unheard of applications in the field of biomedicine, biotechnology and brain research.”

A Dense Array of Sensors Yields More Effective, Accurate Data


The Infineon Neuro-Chip integrates 128 x 128 sensors in an array pattern covering just one square millimeter. A sophisticated electronic circuit is integrated below each sensor, which amplifies and processes the extremely weak signals of neurons. Individual neurons are placed into a nutrient solution above the sensor array, which keeps the neurons alive and allows reconstruction of nerve tissue. Compared to classical methods of research, in which neurons are damaged in the preparation of study samples, undisturbed observation of nerve tissue over a period of several weeks offers scientists a continuous insight into the functionality of how the nervous system and brain learns, processes and stores its learnings.

The sensor density of the Infineon Neuro-Chip is approximately 300 times greater than today’s common methods for studying neurons, which use glass substrates with vapor-deposited metallic lanes to contact the neuron. Each sensor on the chip is separated by a distance of just eight micrometers (a thousandth of a millimeter). Since the typical size of neurons is between 10 - 50 micrometers, low-density sensors may not establish a reliable contact. The high-density sensor array of the Neuro-Chip assures that each neuron in a sample is contacted by at least one sensor.

Instead of sequentially checking every single neuron, the Infineon Neuro-Chip surveys several neurons at the same time. As a result, more statistically relevant data is available. Additionally, the Neuro-Chip enables recording of the operating sequence of electrical activity within nerve tissue over a defined time. Every second, the Neuro-Chip can record more than 2,000 single values for each of its 16,384 sensors. The data can then be transformed into a color picture for visual analysis. Researchers can detect from this data how complete nerve tissues react to electrical stimulation or certain chemical substances in a given period of time.

Analysis and Evaluation on a Third of a Square Centimeter


The total area of Infineon’s Neuro-Chip measures five millimeter by six millimeter, including the circuitry required to amplify and process the neuron signals and transmit the data off-chip. The chip is based on a standard Complementary Metal Oxide Semiconductor (CMOS) technology extended with additional process steps to realize the capacitive sensors array.

Infineon’s successful development of a complete integrated circuit enabling observation of the extremely low cell signals is a world technology breakthrough. The Neuro-Chips can detect and handle voltage changes with peaks ranging from 100 µV (microvolt, one millionth of 1 Volt) to 5 mV (millivolt, one thousandth of 1 Volt).

About Infineon


Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2002 (ending September), the company achieved sales of Euro 5.21 billion with about 30,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.

Information Number

INFCPR200302.041e

Press Photos

  • The "Neuro-Chip" from Infineon Technologies is connected with a living nerve cell. The Neuro-Chip's 16,384 sensors read the electrical activity of the cell. The typical size of neurons is between 10 - 50 micrometers (1 µm, a thousandth of a millimeter).    Press Photo: Infineon Technologies, Max Planck  Institute
    The "Neuro-Chip" from Infineon Technologies is connected with a living nerve cell. The Neuro-Chip's 16,384 sensors read the electrical activity of the cell. The typical size of neurons is between 10 - 50 micrometers (1 µm, a thousandth of a millimeter). Press Photo: Infineon Technologies, Max Planck Institute
    Press Picture

    JPG | 313 kb | 636 x 484 px

  • Microscopic zoom on the Neuro-Chip makes visible the sensor grid of 1 millimeter x 1 millimeter and the circuitry above which enables to record, amplify and process the more than 32 million information bytes presented by the 16,384 sensors on the grid every second.    Press Photo: Infineon Technologies, Max Planck  Institute
    Microscopic zoom on the Neuro-Chip makes visible the sensor grid of 1 millimeter x 1 millimeter and the circuitry above which enables to record, amplify and process the more than 32 million information bytes presented by the 16,384 sensors on the grid every second. Press Photo: Infineon Technologies, Max Planck Institute
    Press Picture

    JPG | 441 kb | 1600 x 1200 px

  • The microscope makes visible the sensor array and circuitry of Infineon's Neuro-Chip. Neurons are placed on the sensor array for further studying.     Press Photo: Infineon Technologies, Max Planck  Institute
    The microscope makes visible the sensor array and circuitry of Infineon's Neuro-Chip. Neurons are placed on the sensor array for further studying. Press Photo: Infineon Technologies, Max Planck Institute
    Press Picture

    JPG | 1.19 mb | 2272 x 1704 px

  • Infineon's Neuro-Chip records and amplyfies the electrical signals from nerve cells, so-called neurons, and transfers them to a computer system for processing. The data can then be transformed into a color picture for visual analysis. Researchers can detect from this data how complete nerve tissues react to electrical stimulation or certain chemical substances in a given period of time.    Press Photo: Infineon Technologies, Max Planck  Institute
    Infineon's Neuro-Chip records and amplyfies the electrical signals from nerve cells, so-called neurons, and transfers them to a computer system for processing. The data can then be transformed into a color picture for visual analysis. Researchers can detect from this data how complete nerve tissues react to electrical stimulation or certain chemical substances in a given period of time. Press Photo: Infineon Technologies, Max Planck Institute
    Press Picture

    JPG | 1.13 mb | 2272 x 1704 px

  • Individual neurons are placed into a nutrient solution above the Neuro-Chip's sensor array, which keeps the neurons alive and allows reconstruction of nerve tissue.    Press Photo: Infineon Technologies, Max Planck  Institute
    Individual neurons are placed into a nutrient solution above the Neuro-Chip's sensor array, which keeps the neurons alive and allows reconstruction of nerve tissue. Press Photo: Infineon Technologies, Max Planck Institute
    Press Picture

    JPG | 353 kb | 1600 x 1200 px

  • With 16,384 tiny sensors packed into one square millimeter and surrounded by processing circuits, each of these "Neuro-Chips" will be used to monitor the electrical activity of living nerve cells. Researchers at Infineon Technologies and the Max Planck Institute for Biochemistry developed the technology to gain insight into basic biological functions.    Press Photo: Infineon Technologies, Max Planck  Institute
    With 16,384 tiny sensors packed into one square millimeter and surrounded by processing circuits, each of these "Neuro-Chips" will be used to monitor the electrical activity of living nerve cells. Researchers at Infineon Technologies and the Max Planck Institute for Biochemistry developed the technology to gain insight into basic biological functions. Press Photo: Infineon Technologies, Max Planck Institute
    Press Picture

    JPG | 377 kb | 1600 x 1200 px