Infineon and Metalink Demonstrate Industry's First Multivendor Interoperability at Supercomm - Standard QAM-VDSL Solutions restate its maturity for mass deployment
Atlanta, June 4, 2002 Infineon Technologies AG (FSE/NYSE: IFX), a leading provider of integrated circuits for advanced communications systems, and Metalink Ltd. (NASDAQ: MTLK), a leader in providing high-performance broadband access chip sets, today announced that they will conduct interoperability demonstrations of their respective standards-based, 4-band QAM VDSL solutions at Supercomm 2002, June 4-6, Atlanta GA.
Infineon and Metalink will demonstrate video streaming over VDSL in their respective booths, Infineon # 23726 and Metalink #22332.
Based on the widely deployed, proven QAM (Quadrature Amplitude Modulation) line coding technology, Infineons and Metalinks VDSL chipsets enable the transport of bandwidth-hungry revenue-generating applications such as high quality video, online interactive gaming and fast Internet access. Supporting ETSI and ANSI band allocation plans (plan 997, 998) the chipsets co-exist with all other xDSL technologies as well as with legacy voice and ISDN services.
QAM VDSL is a standard-compliant and proven, robust technology that enables to reduce total system cost by reducing the overall bill of material (BOM) and shrinking system footprint. Unlike the rival DMT technology, used successfully in ADSL, QAM was developed with VDSL in mind and is better suited for true bundled broadband services. The technology, which is now in its third generation, lowers design complexity at both ends of the network and enables access system vendors to offer high performance field-proven QAM-based VDSL products at competitive costs.
Metalink, a fabless semiconductor company, develops and markets high performance broadband access chip sets used by telecommunications and networking equipment makers. Metalink's broadband silicon solutions enable cost effective, very high speed streaming video, voice and data transmission and delivery throughout worldwide communication networks. The Company's top-level algorithmic designers, along with its leadership in standards bodies worldwide, are establishing Metalink as a leader in the field of broadband access. Metalink continues to implement its strategic growth plan of focusing on high growth video deployment and voice over Digital Subscriber Line (DSL) applications and capitalizing on its industry leading SHDSL and VDSL technologies.
Infineon and Metalink will demonstrate video streaming over VDSL in their respective booths, Infineon # 23726 and Metalink #22332.
Based on the widely deployed, proven QAM (Quadrature Amplitude Modulation) line coding technology, Infineons and Metalinks VDSL chipsets enable the transport of bandwidth-hungry revenue-generating applications such as high quality video, online interactive gaming and fast Internet access. Supporting ETSI and ANSI band allocation plans (plan 997, 998) the chipsets co-exist with all other xDSL technologies as well as with legacy voice and ISDN services.
QAM VDSL is a standard-compliant and proven, robust technology that enables to reduce total system cost by reducing the overall bill of material (BOM) and shrinking system footprint. Unlike the rival DMT technology, used successfully in ADSL, QAM was developed with VDSL in mind and is better suited for true bundled broadband services. The technology, which is now in its third generation, lowers design complexity at both ends of the network and enables access system vendors to offer high performance field-proven QAM-based VDSL products at competitive costs.
About Metalink
Metalink, a fabless semiconductor company, develops and markets high performance broadband access chip sets used by telecommunications and networking equipment makers. Metalink's broadband silicon solutions enable cost effective, very high speed streaming video, voice and data transmission and delivery throughout worldwide communication networks. The Company's top-level algorithmic designers, along with its leadership in standards bodies worldwide, are establishing Metalink as a leader in the field of broadband access. Metalink continues to implement its strategic growth plan of focusing on high growth video deployment and voice over Digital Subscriber Line (DSL) applications and capitalizing on its industry leading SHDSL and VDSL technologies.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2001 (ending September), the company achieved sales of Euro 5.67 billion with about 33,800 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.
Information Number
INFCOM200206.091e