Cypress Signs Agreement with Infineon and Micron to Co-Develop CellularRAM"

Sep 16, 2002 | Market News

New Multi-Generation Family of Low Power PSRAMs Designed for 2.5G and 3G Wireless Handsets

SAN JOSE, Calif., September 16, 2002 – Cypress Semiconductor Corporation (NYSE: CY), Infineon Technologies AG (FSE, NYSE: IFX) and Micron Technology, Inc. (NYSE: MU) today announced that Cypress signed a co-development agreement with Micron and Infineon to collaborate in the development of the specifications for CellularRAM™ memory, a new multi-generation family of low-power Pseudo Static RAM (PSRAM) for wireless handsets.

CellularRAM memory is designed to meet the growing memory and bandwidth demands of future 2.5G and 3G handset designs. In addition to offering a lower cost/bit ratio than current solutions, this new type of Pseudo SRAM features SRAM-pin compatibility, external refresh-free operation and a low-power design. CellularRAM memory is a drop-in replacement for asynchronous low-power SRAM used currently in cell phone designs.

The purpose of this co-development effort is to provide customers with pin- and function-compatible products from multiple sources, based on a jointly developed specification for CellularRAM memory. Each company will design and manufacture the products using their own design and process technology.

“As a contributor in the development of the CellularRAM specifications, Cypress is pleased to formally join Infineon Technologies and Micron Technology - industry leaders in memory - in this co-development effort,” said Mario Martinez, strategic director for Cypress’s Memory Products Division. “CellularRAM memory provides wireless handset designers all the benefits of a DRAM cell - including a more cost-effective, higher-density and low-power consumption solution - using a standard SRAM interface.”

“CellularRAM memory provides designers a cost-effective solution for designing high-performance memory for next-generation wireless applications,” said Mario Fazio, director of strategic marketing for Micron’s Wireless Products. “With its substantial presence in the mobile handset memory market, Cypress will further strengthen the co-development and marketing efforts of CellularRAM.”

“We are excited about the addition of Cypress to the co-development agreement,” said Dr. Ernst Strasser, director of marketing for Infineon’s Graphics and Specialty DRAM. “In addition to creating a third source for the industry, we are confident this cooperation will benefit all next-generation wireless customers seeking an outstanding memory solution for 2.5 and 3G handsets.”

Based on a one-transistor DRAM cell, CellularRAM memory provides significant advances over traditional SRAM and a six-transistor (6T) SRAM cell, leveraging the technology and reduced size of a DRAM cell. These products operate at up to 108 MHz clock rates; run at an initial latency of 60 ns; and can achieve up to 216 MB/s (1.6 Gb/s) of peak bandwidth. CellularRAM memory also features a burst read and write mode that emulates an Intel® W18 and Micron Flash Burst compatible protocol with various I/O voltage options.

Infineon and Micron plan to make several CellularRAM devices available in the next 12 months. The first is a 32 Mb device, organized as 2M x 16 scheduled for initial availability in late 2002. A 16 Mb and 64 Mb device, organized as 1M x 16 and 4M x 16, respectively will follow shortly. All companies are jointly working on the definition of the next generation of the CellularRAM product family, a 128 Mb device, which is targeted for sampling in the second half of 2003.

About Cypress


Cypress Semiconductor Corporation (NYSE: CY) is Connecting from Last Mile to First Mile™ with high-performance solutions for personal, network access, enterprise, metro switch, and core communications-system applications. Cypress Connects™ using wireless, wireline, digital, and optical transmission standards, including Bluetooth, USB, Fibre Channel, SONET/SDH, Gigabit Ethernet, and DWDM. Leveraging its process and system-level expertise, Cypress makes industry-leading physical layer devices, framers, and network search engines, along with a broad portfolio of high-bandwidth memories, timing technology solutions, and programmable microcontrollers. More information about Cypress is accessible online at www.cypress.com.

About Infineon


Infineon Technologies AG, Munich, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. A global player, Infineon operates in the USA from San Jose, California, in the Asia-Pacific region from Singapore and in Japan from Tokyo. Employing about 33,800 people worldwide, the company achieved sales of EUR 5.67 billion in fiscal 2001 (ending September). Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (NYSE) under the ticker symbol IFX. Further information is available at www.infineon.com.

About Micron


Micron Technology, Inc., and its subsidiaries manufacture and market DRAMs, very fast SRAMs, Flash Memory, other semiconductor components, and memory modules. Micron's common stock is traded on the New York Stock Exchange (NYSE) under the MU symbol. To learn more about Micron Technology, Inc., visit its web site at www.micron.com.

“Safe Harbor” Statement under the Private Securities Litigation Reform Act of 1995: Statements herein that are not historical facts are “forward-looking statements” involving risks and uncertainties, including but not limited to: the effect of global economic conditions, shifts in supply and demand, market acceptance, the impact of competitive products and pricing, product development, commercialization and technological difficulties, and capacity and supply constraints. Please refer to the company’s Securities and Exchange Commission filings for a discussion of such risks.

CellularRAM is a trademark of Micron Technology, Inc. in the U.S. and is a trademark of Infineon Technologies outside the U.S. Intel is a trademark of Intel Corporation.

Cypress and the Cypress logo are registered trademarks of Cypress Semiconductor Corporation. “Connectivity from Last Mile to First Mile” and “Cypress Connects” are trademarks of Cypress. All other trademarks are the property of their respective owners.


Editorial Contacts:


Cypress Semiconductor
Agnes Toan
(408) 545-6909
ATN@cypress.com

Micron Technology, Inc.
Echo Chadwick
(208) 368-4400
Echadwick@micron.com

Information Number

INFMP200209.139e