Infineon Announces New Bluetooth Solutions - First Samples of the World's Smallest Single-chip Bluetooth Solution Available

Jun 5, 2001 | Technology Media

Monte Carlo - June 5, 2001 - Infineon Technologies (FSE/NYSE: IFX) today announced four new members of its BlueMoon™ product family: BlueMoon™ Single, BlueMoon™ Single Voice, BlueMoon™ Multimedia and BlueMoon™ BlueStar. With these new products Infineon expands its leadership in semiconductor solutions for short range wireless applications, such as Bluetooth, DECT (Digital Enhanced Cordless Telecommunications) and WDCT (Worldwide Digital Cordless Telecommunications).

”As the Bluetooth market diversifies, Infineon continues to quickly provide specialised Bluetooth solutions for the industry,” said Christian Baumgart, Vice President and General Manager of Infineon‘s Business Unit Short Range Wireless. ”Our goal is to enable our customers to extend their leading position in the fast growing Bluetooth market segments.”

About BlueMoon™ Single

Infineon has now started to sample BlueMoon™ Single, the world’s highest integrated semiconductor solution for the Bluetooth short range wireless technology. This solution combines baseband DSP, radio functionality, memory and software, all integrated into one single-chip and aimed at applications requiring Bluetooth functionality in small form factor such as cellular phones and personal digital assistants.

BlueMoon™ Single complements Infineon’s BlueMoon™ family and targets applications where size is of highest priority. The BlueMoon™ family now is the broadest semiconductor solutions offering worldwide and comprises solutions optimized for each of the main application segments. BlueMoon™ Single combines Infineon’s expertise in radio circuit design with state-of-the-art CMOS technology. The advanced architecture is based on the already proven and Bluetooth V1.1 qualified baseband technology and software from the BlueMoon™ I chipset together with a new high performance radio part realised in CMOS technology. Special measures have been taken to assure highest performance over temperature and minimize spurious emissions of the RF part. The BlueMoon™ Single features integrated ROM-based memory and offers an external Flash-interface for rapid prototyping and pre-production. The Bluetooth V1.1 qualified Link Manager and HCI (Host Controller Interface) is supplied with the IC as firmware. The BlueMoon™ Single integrates a 920 kBaud UART (Universal Asynchronous Receiver Transmitter) for data as well as a dedicated PCM interface for voice.

About BlueMoon™ Single Voice

The BlueMoon™ Single Voice is a turnkey, single-chip solution for headset applications. It comprises a high-performance, full duplex voice codec, power management and charging control as well as the complete headset profile with a customizable man-machine interface.

About BlueMoon™ Multimedia

The BlueMoon™ Multimedia chipset is designed for sophisticated PC and multimedia applications, such as laptops, digital cameras and MP3 players. It integrates an ARM7™ µC and includes a Software API (Application Programmers Interface) enabling host and application SW integration. It supports a wide variety of high-speed interfaces (USB, parallel and serial). Building on standard Bluetooth specifications, the BlueMoon™ Multimedia offers an additional mode for high data rate transmission in combination with Infineon RF transceivers allowing data rates of up to 4 Mbit/s.

About BlueMoon™ BlueStar

The BlueMoon™ BlueStar IP is a fully synthesizable VHDL (Very High Description Language) core together with compilable Link Manager Software in C source code enabling fast and simple integration of Bluetooth functionality into application-specific integrated circuits (ASIC) and high-volume applications, like cellular basebands, PDAs and printers. It is designed for Bluetooth embedded solutions and provides a high degree of flexibility regarding manufacturing process technology, on chip bus architectures and µController support (eg ARM7™, ARM9™ and TriCore™)

Price and Availability

Manufactured in an advanced 0,25 µm CMOS process, the BlueMoon™ Single is available in a small outline LFBGA 81 package measuring a tiny 7 mm x 7 mm. Target customers are being sampled today and volume production start is scheduled for end 2001. The pricing for the BlueMoon™ Single is Euro 7.50 for volumes of 1 Million units. The BlueMoon™ Single Voice and BlueMoon™ Multimedia will be sampled to focus customers in Q3 this year. The pricing for the solutions will be below Euro 10 for volumes over 1 Million units. The BlueMoon™ BlueStar macro IP is today available for integration based on a license model.

About BlueMoon™

The BlueMoon™ product family also includes the Bluetooth V1.1 qualified BlueMoon™ I solution supporting a 920 kBaud UART and a 2 Mbit/s PCM interface ideally suited for modules and Bluetooth adapters, as well as a wide variety of Bluetooth amplifiers for long range class 1 operation.

For all BlueMoon™ members, highest priority was set on manufacturability. Novel design concepts have minimized the number and the cost of the external components.

Infineon Technologies stands for proven delivery performance as well as for high level of quality through its own world class semiconductor fabs with all relevant technologies for Bluetooth chipsets being available in-house.

Infineon has proven its system-on-chip expertise in short range wireless systems and has produced more than 40 million transceiver chips for cordless DECT phones and WDCT systems, which operate in the same frequency bands as Bluetooth (2.4 GHz).

About Infineon

Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2000 (ending September), the company achieved sales of Euro 7.28 billion with about 29,000 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at

*Bluetooth is a trademark owned by its proprietor and used by Infineon Technologies under license.

Information Number


Press Photos

  • Infineon Technologies Announced Expansion of its BlueMoon -Family with four new members: BlueMoon -Single, BlueMoon -Single Voice, BlueMoon Multimedia and BlueMoon BlueStar
    Infineon Technologies Announced Expansion of its BlueMoon -Family with four new members: BlueMoon -Single, BlueMoon -Single Voice, BlueMoon Multimedia and BlueMoon BlueStar
    Press Picture

    JPG | 1012 kb | 1535 x 1063 px

  • Infineon Announces New Bluetooth Solutions - First Samples of the World's Smallest Single-chip Bluetooth Solution Available
    Infineon Announces New Bluetooth Solutions - First Samples of the World's Smallest Single-chip Bluetooth Solution Available
    Press Picture

    JPG | 717 kb | 1535 x 1063 px

Download Service