Infineon Introduces the Industry's Highest Density, Lowest Power Switch-on-a-Chip with Embedded Memory for MTU and Enterprise LAN Applications

Aug 21, 2001 | Market News

San Jose, August 21, 2001 – Infineon Technologies (FSE/NYSE: IFX), a leading supplier of communications IC solutions, today announced it has begun sampling a highly integrated, 24+2G Ethernet switch-on-a-chip with embedded memory. The PLB2224 switch-on-a-chip device offers the highest density, lowest power and smallest footprint on the market, making it ideal for enterprise LAN and multi-tenant unit (MTU) switching applications.

“The MTU market focus is shifting to more efficient use of bandwidth and delivery requirements to address the growing connectivity needs of tenants residing and working within buildings and enterprise LAN users,” said Daniel Wong, vice president of Infineon’s communications group and general manager of the LAN Business Unit. “The embedded DRAM enables our Ethernet switch-on-a-chip to handle more data at faster speeds, and offer a lower system cost.”

In addition, when combined with Infineon’s Octal 10BaseSä Ethernet over VDSL transceiver technology, and the production ready managed switch reference design package, the PLB2224 provides OEMs with a complete, easy to implement system solution for fully managed small form factor Ethernet switches.

According to Gartner Dataquest, the worldwide LAN semiconductor market will grow from US$1.73 billion in 2000 to US$2.2 billion in 2003. The worldwide market for MTU hardware, is expected to grow in the same period from US$274 million to US$2.1 billion.

Infineon’s PLB2224 switch is fabricated in 0.18 micron logic process with embedded memory, and is housed in a 272-pin plastic BGA package. The embedded DRAM replaces up to eight memory devices, reduces power consumption by up to 80 percent and device footprint by 50 percent, resulting in a significantly lower system bill of materials.

Features


The PLB2224 is a 24+2G single chip switch with 12 MB of embedded memory for a packet buffer. The device supports 8K MAC addresses with auto-learning and aging. PLB2224 also offers VLAN and QoS features compliant with the IEEE 802.1p and 802.1Q standard, and includes support for management (EtherStat II, SNMP, RMON). Possible system configurations include fixed; either 24+2G, 48+2G, or stacked (controlled with an I2C interface) with up to 7 devices per stack 168+2G.

Availability


The PLB2224 devices and reference boards are available now. Production quantities will be available in Q4 2001 at a price of US$80 per chip in 10K quantities.

About Infineon


Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2000 (ending September), the company achieved sales of Euro 7.28 billion with about 29,000 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com

Information Number

INFCOM200108.108e

Press Photos

  • Infineon Introduces the Industry's Highest Density, Lowest Power Switch-on-a-Chip with Embedded Memory for MTU and Enterprise LAN Applications
    Infineon Introduces the Industry's Highest Density, Lowest Power Switch-on-a-Chip with Embedded Memory for MTU and Enterprise LAN Applications
    Press Picture

    JPG | 1.14 mb | 1535 x 1063 px