Infineon starts volume production of first full-SiC-module, announces additional devices for its CoolSiC™ family at PCIM
Munich and Nuremberg, Germany – 16 May 2017 – Higher efficiency, increased power density, smaller footprints and reduced system costs: these are the main advantages of transistors based on silicon carbide (SiC). Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is starting volume production for the Easy 1B, the first full-SiC module announced during PCIM 2016. On the occasion of this year’s PCIM in Nuremberg, the company is showcasing additional module platforms and topologies for the 1200 V CoolSiC™ MOSFET family. Infineon is now able to bring the potential of SiC technology to a new level.
“Silicon carbide has reached a tipping point: Taking cost-benefit analysis into account, it is ready for use in a variety of applications,” said Dr. Peter Wawer, Division President Industrial Power Control from Infineon. “In order to make the new semiconductor technology a revolution to rely on, however, it needs a partner like Infineon. Products tailored to the application, our own production capacities, comprehensive technology portfolio and system understanding: these four building blocks have made us the market leader for power semiconductors. We want and will also achieve this with our SiC product portfolio."
The new 1200 V SiC MOSFETs have been optimized to combine high reliability with performance. They show dynamic losses which are an order of magnitude lower than 1200 V silicon (Si) IGBTs. First products will initially support upcoming system challenges in applications such as photovoltaic inverters, uninterruptible power supplies (UPS) and charging/storage systems. The new configurations will also enable revolutionary new solutions in industrial drives, medical technology or auxiliary power supplies in the railway sector in the near future.
One major advantage of the trench technology with the 1200 V SiC MOSEFT lies in an extended robustness. This is due to the lower failure in time (FIT) rate and the short-circuit capability, which can be adapted to the respective application. Thanks to a threshold voltage (V th) of 4 V and the recommended switch-on threshold (V GS) of +15 V, the transistors can be controlled like an IGBT and safely switched off in the event of a fault. The SiC MOSFETs enable very fast switching transients. In addition, Infineon’s technology offers an easy adjustability of the transients via gate series resistors. The EMC behavior can thus be easily optimized.
Already last year, Infineon announced the lead products Easy 1B (Half-Bridge / Booster) as well as the discrete TO-247-3pin and -4pin solutions. The Easy 1B platform is well established and an ideal module platform for fast switching devices. At this year’s PCIM fair, Infineon will be exhibiting additional module platforms and topologies based on the 1200 V SiC MOSFET technology. This extends the performance spectrum of the CoolSiC MOSFETs step by step. Among others, Infineon showcases the following SiC modules:
- Easy 1B with B6 (Six-Pack) topology: the module is characterized by the proven Infineon module configuration with an on-resistance (R DS(ON)) of only 45 mΩ. An integrated body diode ensures a low-loss freewheeling function. The Easy 1B is suitable for applications in the fields of drives, solar or welding technology.
- Easy 2B with Half-Bridge topology: this larger Easy device offers an enhanced performance with an R DS(ON) of 8 mΩ per switch. The low-inductance module concept is ideal for applications with more than 50 kW and fast switching operations. These include solar inverters, quick-charging systems or solutions for uninterruptible power supplies.
- 62 mm with Half-Bridge topology: an additional Half-Bridge configuration featuring even higher power with an R DS(ON) of 6 mΩ per switching function. This module platform offers the possibility of low-inductance connection of systems in the medium power range. A great variety of applications make use of this, including medical technology or auxiliary power supplies in the railway sector, to name a few. Because of the large number of possible applications, Infineon anticipates a rapid spread of this module.
Availability
The lead products introduced at PCIM 2016, Easy 1B and the two discrete devices TO-247-3pin and -4pin, are gradually entering volume production during this year. The Half-Bridge configuration for the Easy 1B is now available. Its market launch is supported by various driver modules and demo boards, which are also available from now on. The new product configurations are available as samples, and the serial start is planned for 2018. More information is available at www.infineon.com/coolSiC.
Infineon at the PCIM 2017
At the PCIM 2017 tradeshow Infineon is presenting leading edge technology for efficient systems in industrial, consumer and automotive applications. Infineon’s demos for powering an energy-smart world are presented at booth #412 in hall 9 (Nuremberg, Germany, 16-18 May 2017). Information about the PCIM show highlights is available at www.infineon.com/pcim.
Information Number
INFIPC201705-053
Press Photos
-
The Easy1B with Six-Pack topology is characterized by the proven Infineon module configuration with an on-resistance (RDS(ON)) of only 45 mΩ. An integrated body diode ensures a low-loss freewheeling function. It is suitable for applications in the fields of drives, solar or welding technology.CoolSic_Easy1B
JPEG | 211 kb | 1712 x 1011 px
-
This larger Easy2B in Half-Bridge topology offers an enhanced performance with an RDS(ON) of 8 mΩ per switch. The low-inductance module concept is ideal for applications with more than 50 kW and fast switching operations. These include solar inverters, quick-charging systems or solutions for uninterruptible power supplies.CoolSic_Easy2B
JPEG | 315 kb | 1796 x 1206 px
-
The 62 mm module in Half-Bridge topology is featuring even higher power with an RDS(ON) of 6 mΩ per switching function. This module platform offers the possibility of low-inductance connection of systems in the medium power range. A great variety of applications make use of this, including medical technology or auxiliary power supplies in the railway sector.CoolSic_62mm
JPEG | 266 kb | 1944 x 1164 px