Mocana Security of Things Platform™ integrates support for the Infineon OPTIGA™ TPM

Sep 7, 2016 | Market News

Munich, Germany and San Francisco, USA – September 7, 2016 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Mocana Corporation take IoT security to the next level. Embedded systems security specialist Mocana integrates support for the Infineon OPTIGA™ TPM (Trusted Platform Module) security controller as a standard feature into its latest Security of Things Platform™.

Developers who choose Mocana’s platform for smart factories, infrastructure, automotive and other security-critical IoT designs can now quickly and easily integrate hardware protection into their devices. In addition, millions of IoT devices that already incorporate OPTIGA TPMs from market leader Infineon could benefit from the advanced security features offered by the Mocana software platform.

The Mocana Security of Things Platform secures manifold aspects of connected devices through a comprehensive collection of services such as pre-boot verification, certificate management, cryptographic engines, secured data transport and secured firmware updates. The platform with integrated support for the OPTIGA TPM family will be available in Q4 2016.

OPTIGA TPMs are standalone security controllers based on the international standards of the Trusted Computing Group (TCG). TPMs protect integrity and authenticity of embedded systems by implementing advanced cryptographic algorithms in hardware. These established devices have been used successfully to provide security in PCs for over 15 years and are increasingly included into different embedded systems. A TPM can be thought of as a “safe” within the system as it is capable of resisting both logical and physical attacks.

“We are very excited to announce that Mocana’s software is compatible with Infineon’s OPTIGA TPM 1.2 chips,” said Dean Weber, CTO at Mocana. “We believe this technology will advance Mocana further as a leader in the embedded security space, being one of the few companies that offer security down to the root of trust, which ensures that IP connected devices and the data they provide can be safe and trusted”.

“Developers can rely on solutions with Infineon’s proven hardware and Mocana’s established software,” said Joerg Borchert, Vice President of the Chip Card & Security Division at Infineon Technologies Americas Corp. “Thus, they can quickly and easily bring to market products and systems that provide the highly advanced levels of protection that these applications demand”.

Infineon makes the Internet of Things (IoT) smart, secure and power efficient. Sensors, controllers, power components and security solutions are the building blocks for all major IoT applications from connected cars to industrial or smart home applications. We help our customers to create sustainable IoT success with benchmarking semiconductor technologies and our system understanding of the automotive, energy and security markets. Further information is available at: www.infineon.com/iot, www.infineon.com/iot-security and www.infineon.com/tpm.

Information Number

INFCCS201609-079

Press Photos

  • OPTIGA™ TPM chips increase the data security of laptops and tablet PCs. Sensitive data such as security keys, certificates and passwords can be stored in the TPM chip separately from the main processor and are hence better protected against hacker attacks.
    OPTIGA™ TPM chips increase the data security of laptops and tablet PCs. Sensitive data such as security keys, certificates and passwords can be stored in the TPM chip separately from the main processor and are hence better protected against hacker attacks.
    OPTIGA_TPM_Chip

    PNG | 1.3 mb | 1500 x 1025 px