Infineon develops chip network for textiles - Intelligence by the meter

May 5, 2003 | Market News

Munich – May 5, 2003 – Researchers from Infineon Technologies AG (FSE/NYSE: IFX) have developed a way to make large textile surfaces such as carpeting or tent cloth “intelligent”. This technology innovation may lead to new products for the monitoring of buildings, the structural control of buildings of all kinds and for use in the advertising industry.

Woven into fabrics, a self-organizing network of robust chips is able to monitor temperatures, pressures or vibrations as required. In addition to the sensor functionality, the fabric can be equipped with tiny light-emitting diodes (LEDs) to provide directional guidance or serve as advertising material. In this manner, the “intelligent” fabric could be used as a motion sensor or fire alarm, or to control burglar alarm and air-conditioning systems. Infineon plans to further develop this technology for the integration of microelectronics in textile surfaces into a fully functional, large-scale “intelligent” fabric over the next two years, together with cooperation partners from the textile industry.

The “intelligent” textiles hardly miss a thing



The microelectronics modules in the concept demonstrator of an “intelligent” floor covering are embedded in the textile structure in the form of a checkerboard. Each chip is connected to its four adjacent “neighbors” by electrically conductive threads, which creates a network that enables the flow of information. The information is forwarded between the chips and can be transmitted to various systems such as fire-alarms, burglar alarm or air-conditioning systems via a data interface. In this manner, an “intelligent” carpeting could e.g. tell the alarm system where a person is located in a room and in which direction he/she is moving. Equipped with woven-in and individually controlled LEDs, the carpet can serve as a guidance system, e.g. to guide visitor streams through public buildings or to direct them to emergency exits if a dangerous situation arises.

The basic technology also can be used in the construction industry or in the production of Zeppelins (airships), balloon envelopes and tent-cloth. Additionally, the water- and heat-resistant chips can be used as sensors in various support structures, such as columns or walls envelopes. The chips can gather information about the condition and the loading of materials, thus permitting the early identification of local defects, breakage or cracks in construction materials or fabrics. This can increase building safety because the detection of defects is no longer limited to individually initiated point inspections. Another potential application would be based on the integration of individually controllable LEDs in Zeppelin (airship) and balloon envelopes or in flags and tent walls, permitting these materials to carry advertising or directional messages.

Robust functionality through self-organization and fault tolerance


Each chip automatically determines its position within the network within fractions of a second after initialization. It is connected to its four immediate chip neighbors by electrically conductive threads and exchanges information with them. This creates a self-organizing, i.e. self-learning network that is even fault-tolerant. If a chip or conductive path fails, the network will automatically locate this fault and immediately reorganize itself: It will find a new path within the overall system via the neighboring chips in order to maintain the information flow. This offers the possibility to cut the “intelligent” carpeting to virtually any shape and size without damaging the electronic network function. The chips can be placed with any spacing between them; however, the closer together they are woven into the textile structure, the more accurate they will work.

About Infineon



Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2002 (ending September), the company achieved sales of Euro 5.21 billion with about 30,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.

Information Number

INFCPR200305.68

Press Photos

  • Cartoon
    Cartoon
    Cartoon

    JPG | 711 kb | 2126 x 1421 px

    Cartoon

    JPG | 24 kb | 160 x 107 px

  • Cartoon (german)
    Cartoon (german)
    Cartoon (german)

    JPG | 688 kb | 2126 x 1421 px

    Cartoon (german)

    JPG | 23 kb | 160 x 107 px

  • Researchers from Infineon Technologies AG have discovered a way to make large textile surfaces such as carpeting or tent cloth "intelligent". This  sets new highlights for the monitoring of buildings, the structural control of buildings of all kinds and for use in the advertising industry. Woven  into fabrics, a self-organizing network of robust chips is able to monitor temperatures, pressures or vibrations as required.
    Researchers from Infineon Technologies AG have discovered a way to make large textile surfaces such as carpeting or tent cloth "intelligent". This sets new highlights for the monitoring of buildings, the structural control of buildings of all kinds and for use in the advertising industry. Woven into fabrics, a self-organizing network of robust chips is able to monitor temperatures, pressures or vibrations as required.
    Intelligent Carpet

    JPG | 599 kb | 2126 x 1417 px

    Intelligent Carpet

    JPG | 22 kb | 160 x 107 px