Internet Access via Satellite - Infineon Helps Deliver Broadband at up to 200 Times Dial-up Rates to Practically Anywhere

Nov 27, 2003 | Market News

Munich, Germany – November 27, 2003 – Infineon Technologies (FSE/NYSE: IFX) has created a cost-effective solution for fast access to state-of-the-art broadband services in residential and office buildings. The solution, which is called ‘Constellation’, uses Infineon’s VDSL (Very High Bit-Rate DSL) technology to provide up to 200 times faster in-building transmission rates for Internet, video and multimedia applications. Since the data is transmitted via satellite the solution can be deployed anywhere in the world and can be installed in just a few hours. It provides apartment buildings, office complexes, hotels or hospitals away from population centers with cost-effective access to high-speed Internet, multimedia applications and corporate networks.

Many apartment and business buildings are too far away from a central office to use existing phone wiring for broadband access to the building or would require heavy investment in new infrastructures such as fiber-optic cabling. Therefore telecommunication operators have been looking for a quick-to-install and cost-effective solution. Together with its partners ViaSat in the U.S. and ZyXEL in Taiwan, Infineon developed the ‘Constellation’ solution, which overcomes these obstacles by providing broadband access to the building via satellite. Within a building, the data is distributed with Infineon’s patented VDSL technology via the existing telephone copper wiring. By deploying ‘Constellation’ the time to download a file of 10 MB size could be reduced to a few seconds compared to around 20 minutes with a conventional 56k modem.

The system is ready for operation in just a few hours as it uses wireless satellite access and the existing copper wiring in the building. This is a major benefit for operators who are now able to offer low-cost broadband access to their customers outside of major population centers. In high-density areas ‘Constellation’ can be a competitive alternative as well since it requires only subscriber- and demand-specific investments into the customer equipment.

How Constellation works



The combined data flow for the entire residential or commercial building is received and sent through ViaSat's two-way broadband LinkStar® satellite terminal. A receiver centrally installed in the building converts the data received via satellite into the VDSL format and transmits it via the existing phone wiring to the customer premises modems. Both the switches as well as the modems are supplied by ZyXEL and are equipped with Infineon’s VDSL chipsets.

The transmission of broadband data via common copper-wire phone lines is made possible by Infineon’s VDSL chipset. The chipset is specifically designed for multi-dwelling units and commercial buildings and millions of them have been installed in recent years in switches and modems.

The ‘Constellation’ package is promoted by ZyXEL and ViaSat. The solution operates worldwide in all areas in reach of satellite and is supplied in the form of individual packages according to the number and needs of subscribers in multi-unit residential and commercial buildings.

About Infineon



Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2003 (ending September), the company achieved sales of Euro 6.15 billion with about 32,300 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.

Information Number

INFCOM200311.016