英飞凌推出两个低成本8位微控制器系列,支持驱动、自动化和照明解决方案以及人机界面的高能效设计
Technology Media
2010年3月2日
2010年3月2日,德国纽必堡——在纽必堡举行的2010年嵌入式技术展会上,英飞凌科技股份公司(FSE:IFX / OTCQX:IFNNY)今日推出两个功能强大的全新器件系列,壮大其经济高效并可扩展的XC800微控制器(MCU)产品组合。全新的XC82x 和XC83x系列经过专门设计,可进一步降低系统成本,并改进多种工业产品的能效。
在设计风扇、水泵、压缩机、新型照明解决方案和任何电源转换器的电机控制器时,主要目标是提高能源效率,降低系统成本。采用智能控制概念并与各种通信接口连接,有助于充分满足这些需求。英飞凌通过XC82x 和 XC83x8位微控制器系列,将行业标准的8位8051 CPU与优化的外设进行了有机结合,确保以极低的运行成本,大幅降低能耗。此外,在这两个全新系列中,有几款器件还具备特殊的特性,可改进人机界面的设计,比如触摸屏和LED显示器。
得益于不足0.40欧元(10万枚订购量)的低成本,XC82x 和 XC83x微控制器可确保以极其经济划算的方式,实现节能控制理念。XC82x 和 XC83x微控制器具备多种特性,包括容式触控感应和 LED矩阵控制器、EEPROM 仿真、10位模数转换器(ADC)、与ADC实现硬件连接的捕获比较单元(CCU6)、窗界看门狗定时器、掉电模式和UART、高速SPI 及I2C等通信接口。XC82x系列还集成了乘除算法单元(MDU)。XC83x具备一个16位矢量计算器和一个实现磁场定向控制功能的ROM库及大电流焊盘(30mA 至50mA)。
“除电机控制外,功能强大的智能微控制器有助于大幅改进照明装置、空调和电磁炉的能效,节能潜力达到40%或以上。”英飞凌微控制器市场部总监Juergen Hoika指出,“英飞凌XC82x 和XC83x系列这样的低成本、易用微控制器,有助于系统设计者采用复杂的控制方法,设计出高能效的产品。”
这两个微控制器系列都具备多种特性:生成高分辨率脉宽调制信号,实现快速ADC测量、自主式外设、用于控制回路和保护的比较器,使设计者能够通过采用8位微控制器设计出高能效的产品。尤其是,XC82x/XC83x微控制器具备一个时钟频率为48MHz的捕获比较单元(CCU6)和一个快速16MHz ADC。这个ADC的采样时间仅为125ns,转换时间约为820ns。在设计中,ADC与CCU6直接通过硬件连接,可确保快速、可靠的控制回路。此外,集成的ADC限值检验器还具备8位数字比较器的功能。
缩短工业产品的开发周期
英飞凌提供多种应用套件和工具,满足新系统设计的关键上市时间要求。利用inDrive800,英飞凌可提供适用于驱动器和自动化产品的全套8位解决方案,帮助缩短产品的开发周期。工程师无需从头开始,可在英飞凌应用套件的基础之上进行设计。英飞凌的应用套件分为不同的功率等级,并采用多种功能方案。免费的IDE和工具链便于轻松选择和配置所需的微控制器及重复使用特定应用的源代码。
利用inTouch800,英飞凌可为高度集成的人机界面提供XC82x 和XC83x系列解决方案。利用一个24引脚微控制器管理容式触摸控制和LED显示屏或步进式仪器的操作,,无需驱动设备。
成本敏感型产品需要易用、免费的工具。为此,英飞凌今日宣布推出DAVE™ Bench——英飞凌微控制器开发工具平台。适用于XC800系列的第一版开发平台包括一个基于Eclipse的IDE、DAVE连接器、SDCC C编译器、HiTOP一级调试器、闪存加载程序和UART终端U-SPY(包括数据显示)。
此外,英飞凌的开发工具合作伙伴Keil将提供新版本C51编译器。“英飞凌XC800系列具备提高工业、汽车和其他嵌入式产品能效的功能。”ARM德国有限公司微控制器开发工具负责人Reinhard Keil指出,“英飞凌的XC82x和XC83x系列扩大了成本敏感的嵌入式应用的器件的范围,有助于提升Keil C51编译器的性能和代码密度。”
供货与定价
XC82x 和 XC83x系列有多种不同的型号,可编程闪存容量从2KB到8KB不等,采用16引脚至28引脚等不同的封装形式,工作温度高达125 °C。该产品组合还包含符合汽车应用的ACQ100标准要求的专用器件。若订购量达到10万枚,单价为0.39欧元(0.55美元)至0.72欧元(1.01美元)。XC82x系列的工程样品目前已提供,XC83X系列的工程样品预计将于2010年4月开始提供。
更多信息
在纽必堡举行的2010年嵌入式技术展会(2010年3月2日至4日)上,英飞凌将在公司的展台(21号展厅的428号展台)展出其全新的微控制器、全新的软件开发平台DAVE Bench、具备触控感应和LED演示功能的全新Easy Kit及inTouch800演示套件。
英飞凌微控制器的更多信息可在
www.infineon.com/microcontrollers找到。
About Infineon
总部位于德国纽必堡的英飞凌科技股份公司,为现代社会的三大科技挑战领域——能源效率、通讯和安全性提供半导体和系统解决方案。2009财年(截止到9月份),公司实现销售额30.3亿欧元,在全球拥有约25,650名雇员。英飞凌科技公司的业务遍及全球,在美国苗必达、亚太地区的新加坡和日本东京等地拥有分支机构。英飞凌公司目前在法兰克福股票交易所(股票代码:IFX)和美国柜台交易市场(OTCQX)International Premier(股票代号:IFNNY)挂牌上市
更多信息请访问
www.infineon.com。
本新闻稿还可从
www.infineon.com/press/找到。
Information Number
INFATV201003.038
| Press Photos | |
|---|---|
Image |
Description |
![]() |
Infineon expanded its cost-effective and scalable XC800 microcontroller (MCU) portfolio with two powerful new device series: With the XC82x and XC83x series of 8-bit microcontrollers Infineon combines the market standard 8-bit 8051 CPU and peripherals optimized to enable high energy savings at very low implementation costs.
|
![]() |
Infineon expanded its cost-effective and scalable XC800 microcontroller (MCU) portfolio with two powerful new device series: With the XC82x and XC83x series of 8-bit microcontrollers Infineon combines the market standard 8-bit 8051 CPU and peripherals optimized to enable high energy savings at very low implementation costs.
|
![]() |
Juergen Hoika, Marketing Director, Microcontrollers at Infineon Technologies AG
|
| Name | Contact | ||
|---|---|---|---|
|
Monika Sonntag Media Relations |
|