英飞凌XMC4500工业单片机和全面的开发工具套件现已供货

2012-2-28 | 技术媒体

2012年2月28日,德国纽必堡和纽伦堡讯 — 英飞凌科技股份公司(FSE:IFX / OTCQX:IFNNY)已发布XMC4500系列产品。这是英飞凌推出的首个基于ARM® Cortex™ M4处理器的32位工业单片机产品家族。XMC4500单片机将于2012年5月投入量产。目前,英飞凌正携XMC4500单片机样品,隆重参加在德国纽伦堡举办的“2012年国际嵌入式系统展”。为 该产品锦上添花的是一套可提供全面支持的开发工具:除英飞凌免费提供的DAVE™ 3开发环境之外,还提供了包括编译器、调试器、软件分析和Flash烧录工具等在内的全套工具,以 及知名供应商提供的范围广泛的软件解决方案和咨询服务。XMC4500系列特别适用于电力传动、太阳能逆变器以及工业自动化和楼宇自控等应用。

英飞凌科技股份公司工业与多元市场部负责单片机业务的高级主管Stephan Zizala博士表示,“相比于其他竞争产品,度身定制的XMC4000家族更加贴合工业客户的特定要求:它 提供了高性能外设和全面的开发环境,便于设计人员轻松上手,节省宝贵的时间,并且完全免费。在XMC4500系列的设计过程中,英飞凌充分发挥了30多年来在开发面向工业应用的单片机方面积累的丰富经验。X MC4500拥有专为电机控制而优化的定时器模块以及快速ADC、集成式Delta-sigma解调器、强大而快速的Flash存储器等特性,并且工作温度范围更宽,最高可达125°C。”

同XMC4000家族的所有成员一样,XMC4500系列有助于提高系统能效,可支持大量通信标准,并且降低了软件开发的复杂度。为此,英飞凌免费提供了集成式DAVE 3开发环境。除 基于DAVE应用生成代码之外,DAVE 3开发环境还配备了GNU编译器、调试器和数据可视化工具等。英飞凌还可提供模块化设计应用套件。取决于不同的应用要求,可将最多三个分别用于实现与其他系统的通信、支 持执行器和传感器以及提供人机接口(HMI)功能的卫星板,连接至中央CPU板。

主频为120MHz的中端XMC4500系列
目前,XMC4500系列包含若干个产品型号,这些产品具备不同的工作温度范围(85 °C或125 °C)、Flash存储容量(512 kB到1 MB不等)和封装( LQFP-100、LQFP-144和LFBGA-144)。XMC4500单片机搭载时钟频率为120 MHz的CPU、160 KByte的RAM以及丰富的外设和接口。外 设包括4个12位快速并行模数转换器模块、两个12位数模转换器模块、4个Delta-sigma解调器模块和6个捕捉/比较单元(CCU4和CCU8)。除此之外,还有两个定位接口模块、一 个触控和一个LED矩阵控制模块。通信功能则包括以太网、USB和SD/MMC等接口。此外,还提供了3个CAN节点、6个串行通信通道和一个外部总线接口。

XMC4500的供货和定价情况
现已可在“2012年国际嵌入式系统展”上订购XMC4500系列样品。取决于所选择的CPU工作频率、工作温度范围和封装等,X MC4500单片机的单价在3.90欧元到5.50欧元不等(订货量达一万颗时)。

其他XMC4000家族成员的供货情况
XMC代表“跨市场的单片机”,正如其名,XMC4000家族适于应用在广泛的工业产品中。目前,XMC4000家族包含5个系列。这几个系列主要在内核频率、内存容量、外 设功能以及I/O端口数量等方面各不相同:XMC4500采用了120 MHz CPU(现已可提供样品)、XMC4100和XMC4200采用了80 MHz CPU、XMC4400采用了120 MHz CPU,而采用180 MHz CPU的XMC4700系列则尚在设计阶段。将从2012年第四季度开始提供XMC4400、XMC4200和XMC4100系列的样品。

更多信息
如欲了解关于XMC4500系列和XMC4000家族的更多信息,请访问 www.infineon.com/xmc和2012年1月23日发布的新闻稿。
如欲了解关于为我们提供工具的合作伙伴的信息,请访问 www.infineon.com/xmc-swt

在2012年2月28日至3月1日在德国纽伦堡举办的“2012年国际嵌入式系统展”上,英飞凌将在4号厅142号展台上展出其XMC4500系列和DAVE 3开发环境。关 于英飞凌在本届展会上的其他精彩亮点,请访问www.infineon.com/embeddedworld。

About Infineon

总部位于德国纽必堡的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、移动性和安全性提供半导体和系统解决方案。2011财年(截止到9月30日),公司实现销售额40亿欧元,在 全球拥有约26,000名雇员。英飞凌科技公司的业务遍及全球,在美国苗必达、亚太地区的新加坡和日本东京等地拥有分支机构。英飞凌公司目前在法兰克福股票交易所(股票代码:IFX)和美国柜台交易市场( OTCQX)International Premier(股票代号:IFNNY)挂牌上市。

更多信息请访问 www.infineon.com

本新闻稿还可在 www.infineon.com/press/上找到。


Information Number

INFATV201202.028

Press Photos

  • The XMC4500 series is the first device in the 32-bit XMC4000 family on to market. It uses the ARM® CortexT-M4 processor
    The XMC4500 series is the first device in the 32-bit XMC4000 family on to market. It uses the ARM® CortexT-M4 processor
    XMC4500

    JPG | 461 kb | 1800 x 1328 px

  • The modular design kit for the XMC4500 series. Up to three additional application boards - for actuators and sensors (top), for human-machine interface (HMI) functions (right), and for communication with other systems (left) - can be connected to the basic design board with XMC4500 (middle), depending on the respective application requirements.
    The modular design kit for the XMC4500 series. Up to three additional application boards - for actuators and sensors (top), for human-machine interface (HMI) functions (right), and for communication with other systems (left) - can be connected to the basic design board with XMC4500 (middle), depending on the respective application requirements.
    Application_Board_Kits

    JPG | 624 kb | 2126 x 1535 px

  • Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AG
    Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AG
    Zizala_Stephan

    JPG | 1.63 mb | 1535 x 2126 px