Shareholder Structure

Sec. 21 of the German Securities Trading Act (Wertpapierhandelsgesetz – “WpHG”) requires each person whose shareholding reaches, exceeds or, after exceeding, falls below the 3%, 5%, 10%, 15%, 20%, 25%, 30%, 50% or 75% voting rights thresholds of a listed corporation to notify such to the corporation and to the German Federal Supervisory Authority for Financial Services (Bundesanstalt für Finanzdienstleistungsaufsicht - "BaFin") immediately, but no later than four trading days after they have reached, exceeded or fallen below such a threshold. For the purpose of determining the relevant shareholding, voting rights which are deemed to be held by way of attribution according to sec. 22 WpHG must also be taken into consideration. Non-compliance with the notification requirement has serious consequences: such holders cannot exercise any rights from any of the shares concerned until the disclosure requirement has been complied with (and in certain cases six months longer). In addition, a fine of up to € 2 million can be imposed on the relevant shareholder; regarding legal entities even a fine of up to 10 million or 5 per cent of the relevant (group) turnover of the reportable legal person may be imposed.

The voting rights held by the investors listed in the following table are taken from the respective latest shareholder notification to Infineon. The stated percentages in the second column refer to the number of shares on which the notification has been based.

Total voting rights as of April 28, 2017: 1,135,271,687 shares
Free float: 99.47%
Investor relating to the number of shares on which the notification has been based

Allianz Global Investors GmbH

5.74% 
(as of Nov 26, 2015, relating to 1,129,271,481 shares)

BlackRock, Inc.

5.14% 
(as of Apr 03, 2017, relating to 1,135,201,707 shares)

 (Status: April 28, 2017)

Publication of Shareholder Notifications

According to sec. 26 of the German Securities Trading Act Infineon is obligated to disclose notifications of voting rights made pursuant to sec. 21, 22 and 25 and 25a WpHG. We comply to this obligation by using the Internet platform of DGAP (Deutsche Gesellschaft für Ad-hoc-Publizität mbH). The complete wording of these disclosures is available here.

Changes of Address in Share Register

Infineon shareholders can arrange online for a change in their address to be noted in the official share register (by clicking on "Shareholder" on the link below).

registrar services GmbH