Letter to the Shareholders
Fiscal Year in Review
The IFX Share
Concentration
  Convergence
  Confidence
   
   
 

 


Since September 2000, share prices of all chip manufacturers have been on a sharp downslide. Infineon has been no exception. The downturn set in as it became clear that growth expectations for technology markets and stocks had been too high. Falling revenues and earnings in the semiconductor industry caused by the rapid decline in consumer demand - which was initially reflected by the "early warning system" of memory chips for PCs, later on by chips for mobile communications and networking - exerted even more downward pressure on the share prices of the semiconductor manufacturers.

Moreover, the global economy deteriorated steadily in 2001: in particular because of slower economic growth in the U.S., the cutbacks in capital spending among businesses, especially in the telecommunications industry, and the slump in semicon-ductor prices due to overly high inventories. The consequence: A 72 percent drop in share prices of chip manufacturers and thus of the leading U.S. index, namely SOX (Philadelphia Semiconductor Index), starting at its peak in March 2000 and decreasing until September 2001. At the same time, the DAX, which is the leading German index, dropped 46 percent, a clear sign of the downturn in business confidence.

 

Fiscal Year 2000 2001
Stock price performance (Xetra)
   
All-time high
EUR 93.60 EUR 58.25
All-time low
EUR 49.50 EUR 11.52
Closing price (end of September)
EUR 54.88 EUR 13.50
Average daily trading volume
2,304,229 3,121,172
thereof in Xetra Trading System
(80%) (91%)
Number of shares outstanding and market capitalization
   
Shares outstanding (weighted average)
614m 641m
Shares outstanding (as of September 30)
625.5m 693m
Market capitalization (as of September 30) EUR 34,327m EUR 9,356m

(Quelle: Bloomberg)




Search
HelpSelect
Select your language
HelpSelect